Bridge across networks

Use a bridge to connect two networks and, if necessary, convert communications from one network protocol to another so that they can communicate. Creating a bridge in the
Network Browser
enables the browser to detect devices on another physical network and enables users to perform diagnostic and configuration functions on those devices. After adding a bridge, the name given to the bridge appears in the
Network Browser
tree topology.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal