Add New dialog box settings

When adding a bridge, define the name and target bridge network using the
Add New
dialog box.
Setting
Description
Name
Used to create a name for the bridge. Names can include letters, numbers, spaces, and special characters.
Select Target Bridge Network
Used to select a device that has two communication ports for two different networks or a separate device in the same chassis to connect with a different network.
Copy Setting From
Used to copy an existing configuration path into the new bridge. If there is not an existing configuration path, empty will appear in the list.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal