Add New dialog box

How do I open the Add New dialog box?
  1. In the
    Network Browser
    click
    Advanced Settings
    Advanced Settings.
  2. In the
    Advanced Settings
    dialog box, click
    Bridged
    .
  3. Click
    Add New
    .
Use the
Add New
dialog box to:
  • Create a name for a new bridge
  • Select a target path for a new bridge
  • Copy an existing configuration path into a new bridge
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal