Bridge Path Selection dialog box

How do I open the Bridge Path Selection dialog box?
  1. In the
    Network Browser
    click
    Advanced Settings
    Advanced Settings.
  2. In the
    Advanced Settings
    dialog box, click
    Bridged
    .
  3. Click
    Add New
    .
  4. From the
    Add New
    dialog box, in
    Name
    , enter a name for the bridge.
  5. Click
    Browse
    (...) next to the
    Select Target Bridge Network
    box.
The
Bridge Path Selection
dialog box includes the devices from the network topology tree in the
FactoryTalk Linx
Browser
. In the
Bridge Path Selection
dialog box, select the network to connect to the current network.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal