Edit a bridge

Edit a bridge to update settings and change the IP addresses for devices in the bridge configuration.
To edit a bridge
  1. In the
    FactoryTalk Linx
    Network Browser
    , below a bridged module, select the Ethernet network branch, and then click the Property icon Property icon.
    小贴士:
    You can also edit a bridge from the
    Bridged
    tab in the
    Advanced Settings
    dialog box.
  2. In the
    Bridge Configuration
    dialog box, click the Advanced tab and configure the tuning settings to change how fast the
    FactoryTalk Linx
    Network Browser
    discovers items on the network.
  3. Click
    Apply
    .
  4. Click the
    General
    tab.
  5. Click
    Add New
    .
  6. To remove an IP address or range from the list, select the checkbox next to the address and click
    Delete
    .
  7. To modify the information for an existing IP address or range in the list, select an item in the list and then edit the associated properties.
  8. Click
    OK
    to save the changes.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal