Delete a bridge

Deleting a bridge removes the connection between devices on a bridged network. If devices on a bridged network are no longer valid, delete the bridge in the
Network Browser
.
To delete a bridge
  1. In the
    Network Browser,
    below a bridged module, locate the Ethernet branch.
    小贴士:
    You can also delete a bridge from the
    Bridged
    tab in the
    Advanced Settings
    dialog box.
  2. Click the
    Delete
    Delete icon icon to delete the bridge.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal