Add a bridge

Create a bridge to enable the
FactoryTalk Linx
Network Browser
to detect devices on another network and perform diagnostic and configuration functions on those devices.
To add a bridge
  1. In the
    FactoryTalk Linx
    Network Browser,
    below a bridged module, click the Ethernet network branch, and then click the Property icon
    Property
    icon.
    小贴士:
    You can also add a bridge from the
    Advanced
    tab in the
    Advanced Settings
    dialog box.
  2. In the
    Bridged Configuration
    dialog box, click
    Add New
    .
  3. From the
    Add New
    dialog box, in the
    Name
    box, enter a name for the bridge.
  4. Next to the
    Select Target Bridge Network
    box, click
    Browse
    (...).
  5. From the
    Bridge Path Selection
    dialog box, select a device for the
    FactoryTalk Linx
    Browser
    to detect on another network.
    小贴士:
    To add an existing configuration path from another bridge instead of creating a new target bridge path, click the
    Copy Setting From list
    and select a configuration. If there are no existing configuration paths to select,
    Empty
    is displayed in the
    Copy Setting From
    list.
  6. Click the
    General
    tab and configure the browsing discovery options for the bridge.
    • Enable Automatic Discover
    • Make Discovery Continuous
    • Show unrecognized devices
  7. Click
    OK
    to save.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal