Bridge Configuration dialog, General

The
General
tab on the
Bridge Configuration
dialog box contains this information:
Setting
Description
Name
The descriptive name for the bridge. Adding a descriptive name for a bridge makes it easier to find the bridge in the
Network Browser
network topology tree. The name can contain characters, including letters, numbers, and special characters.
Device Serial Number
The unique identification number of the device.
Port Number\IP Address
The downstream IP address and port number of the bus node help identify a unique bridge configuration.
No.
Indicates the number of an item in the list.
Device List/Range
A list of items in the applicable range. Select the check box next to an item in the
Device List/Range
to edit the item settings.
Pencil Icon
Used to modify an IP address.
Add New
Used to add a new item to the list.
Delete
Used to delete an item from the list.
Copy
Used to copy an item(s) in the list.
Paste
Used to paste an item(s) in the list.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal