Copy a device configuration

To copy a device configuration in a bridge
  1. In the
    FactoryTalk Linx
    Network Browser
    click
    Advanced Settings
    Advanced Settings.
  2. In the
    Advanced Settings
    dialog box, click
    Bridged
    .
  3. Select the device in the applicable bridge configuration and click
    Add New
    .
  4. In the
    Add New
    dialog box, click the
    Copy setting From
    list and select the bridge that contains the desired device.
  5. Click
    Browse
    Browse button next to
    Select Target Bridge Network
    to open the
    Bridge Path Selection
    dialog box.
  6. Select the desired device and click
    OK
    .
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal