Upload and register a device description file in the Network Browser

Upload and register device description files of devices within the
FactoryTalk Linx
Network Browser
.
For an online device in the network topology tree, if there is a device description file within the device's firmware, you can upload the device description file in the
FactoryTalk Linx
Network Browser
and register it to the
FactoryTalk Linx
data server. Once registered, the device information shows in the
FactoryTalk Linx
Network Browser
, and communications to other information within the device are possible.
Use the
FactoryTalk Linx
Network Browser
to:
  • Manually upload and register a device description file
  • Automatically upload and register a device description file
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal