Considerations when uploading and registering device description files

To manually or automatically upload and register device description files in the
FactoryTalk Linx
Network Browser, consider the following:
  • This function updates the device description files on the computer that hosts the
    FactoryTalk Linx
    data server. Once registered, the device description file is available for use in client computers that exchange data with the
    FactoryTalk Linx
    data server.
  • To support a new device on computers with different
    FactoryTalk Linx
    data servers, you must register the hardware device's device description file on each target computer respectively.
  • Some hardware devices, such as
    Data Highway Plus
    (DH+) devices, do not have device description files and therefore do not support upload and registration.
  • Some hardware devices, such as Micro800 series devices and
    PanelView Plus
    terminals, require a patch or a new release of
    FactoryTalk Linx
    that officially adds support for the new hardware devices. These devices cannot communicate with
    FactoryTalk Linx
    merely by device description file upload and registration.
  • If a device description file is invalid, or an error occurs during the upload and registration, the device description file cannot be registered, and a diagnostics message is logged into
    FactoryTalk Diagnostics
    Viewer. To view the diagnostics messages:
    • From the Windows
      Start
      menu, select
      All Programs > Rockwell Software > FactoryTalk Tools > Diagnostics Viewer
      , or
    • In
      FactoryTalk Administration Console
      , from the
      Tools
      menu, select
      FactoryTalk Diagnostics
      > Viewer
      .
  • If you upgrade or reinstall
    FactoryTalk Linx
    , the device description files that are previously registered on your computer are lost. You must register the device description files again.
To automatically upload and register device description files in the
FactoryTalk Linx
Network Browser, consider the following:
  • If the EDS / Device Description Auto Upload function is enabled, the system detects and uploads device description files from the child devices of a selected node. If a selected node contains a grandchild device, the grandchild device's device description file is not uploaded automatically. To upload and register a device description file from a grandchild device, select its upper-level node to ensure the automatic browsing and uploading, or right-click the device in the network topology tree and select
    EDS / Device Description Upload
    .
  • The EDS / Device Description Auto Upload function only uploads and registers device description files for unknown devices. If an existing device contains a new device description file, the system does not upload and register it. To update the new device description file, right-click the existing device in the network topology tree and select
    EDS / Device Description Upload
    .
  • If there are many device description files being registered, the
    FactoryTalk Linx
    Network Browser
    may respond slowly.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal