Device monitor mechanism

The service will scan devices by group in turn to collect data. After all devices in a group are scanned, there is a group interval. Once all devices have been scanned, the service will start a cycle interval. The service will return the latest scanned data during data subscriptions. This process is not associated with the
Interval between update cycles
configuration on the General tab. A device will be monitored only when the client subscribes it.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal