Device counters

The following are the device counter's parameters and their meanings. These counters are associated with the service configuration.
Parameter
Description
Type
Address
Shows the device address, such as IPv4, hostname, or DNS.
Text
AliasName
Shows the device address's alias name. This counter is the user-assigned name for the device that is set in the configuration in FactoryTalk Administration Console.
Text
ConnectionStatus
Shows the connection status. For more information, see Status code.
Numeric
ConnectionStatusCode
Shows the connection status code.
The code is returned by the Windows ICMP service.
For more information, see Status code.
Numeric
LastPingAttemptTime
Shows the last attempt time to ping the device. For example: 2024-8-8 16:08:48.5293961
String
LastPingFailureTime
Shows the last failure time to ping the device. For example: 2024-8-8 16:08:48.5293961
String
LastPingSuccessTime
Shows the last success time to ping the device. For example: 2024-8-8 16:08:48.5293961
String
PingDiagnosticReset
Resets the device counter. Once a client is connected to the FactoryTalk Resource and Status server, you can change the
PingDiagnosticReset
value to 1 to reset these device counters, and then the service will reset the value to 0 automatically:
  • PingQuantityAttempts
  • PingQuantityFailures
  • PingQuantitySuccess
Bool
PingQuantityAttempts
Shows the attempts number of pinging devices.
Numeric
PingQuantityFailures
Shows the failure number of pinging devices.
Numeric
PingQuantitySuccess
Shows the success number of ping devices.
Numeric
RefreshPingStatus
Starts a data update cycle immediately.
Bool
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal