Status code

The following are the address' status codes and their meanings. The code is returned by the Windows ICMP service. For more information, see ICMP_ECHO_REPLY (ipexport.h) - Win32 apps | Microsoft Learn.
Status code
Value
Meaning
IP_SUCCESS
0
The status was success.
IP_BUF_TOO_SMALL
11001
The reply buffer was too small.
IP_DEST_NET_UNREACHABLE
11002
The destination network was unreachable.
IP_DEST_HOST_UNREACHABLE
11003
The destination host was unreachable.
IP_DEST_PROT_UNREACHABLE
11004
The destination protocol was unreachable.
IP_DEST_PORT_UNREACHABLE
11005
The destination port was unreachable.
IP_NO_RESOURCES
11006
Insufficient IP resources were available.
IP_BAD_OPTION
11007
A bad IP option was specified.
IP_HW_ERROR
11008
A hardware error occurred.
IP_PACKET_TOO_BIG
11009
The packet was too big.
IP_REQ_TIMED_OUT
11010
The request timed out.
IP_BAD_REQ
11011
It was a bad request.
IP_BAD_ROUTE
11012
It was a bad route.
IP_TTL_EXPIRED_TRANSIT
11013
The time to live (TTL) expired in transit.
IP_TTL_EXPIRED_REASSEM
11014
The time to live expired during fragment reassembly.
IP_PARAM_PROBLEM
11015
It was a parameter problem.
IP_SOURCE_QUENCH
11016
Datagrams are arriving too fast to be processed and datagrams may have been discarded.
IP_OPTION_TOO_BIG
11017
An IP option was too big.
IP_BAD_DESTINATION
11018
It was a bad destination.
IP_GENERAL_FAILURE
11050
It was a general failure. This error can be returned for some malformed ICMP packets.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal