Data from FactoryTalk Diagnostics Counter Monitor

FactoryTalk Resource and Status server gets FactoryTalk Diagnostics Counter Monitor data from:
  • FactoryTalk Linx
  • FactoryTalk Linx Instance02
  • FactoryTalk Linx Gateway OPC UA Server
  • FactoryTalk Linx Gateway OPC DA Server
  • FactoryTalk Linx Gateway RTD Server
  • FactoryTalk Linx Gateway DDE Server
  • FactoryTalk Linx Gateway MQTT
小贴士: FactoryTalk Linx and the FactoryTalk Linx OPC UA Connector also provide diagnostic information as predefined tags associated with a data source they are configured to interface with.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal