Data from workstations

The following are the data from workstations. This information can normally be found by accessing the Windows operating system Task Manager’s
Performance
tab.
Component
Parameter
Description
Type
Unit
CPU
Processes
Shows the number of processes using the server host's CPU. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
N/A
SpeedMHz
Shows the CPU speed. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
Megahertz
UtilizationPercent
Shows the CPU usage percent. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
Percent
Disk
TotalGB
Shows the total space of all computer's hard disks. This attribute is retrieved from Windows and can be viewed in the Windows
File Explorer
.
Numeric
Gigabyte
TotalGB.C
Shows the total space of drive C. C means the drive name. If the multiple drives in a computer are monitored, all drives will be listed. This attribute is retrieved from Windows and can be viewed in the Windows
File Explorer
.
Numeric
Gigabyte
UsedGB
Shows the used space of all computer's hard disks. This attribute is retrieved from Windows and can be viewed in the Windows
File Explorer
.
Numeric
Gigabyte
UesedGB.C
Shows the used space of drive C. C means the drive name. If the usage for multiple drives in a computer is monitored, all drives will be listed. This attribute is retrieved from Windows and can be viewed in the Windows
File Explorer
.
Numeric
Gigabyte
Memory
AvailableGB
Shows the amount of memory which is available for allocation to a new process or to existing processes. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
Gigabyte
CommitedGB
Shows the physical memory in use for which space has been reserved in the paging file should it need to be written to disk. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
Gigabyte
InuseGB
Shows the amount of memory being used by applications. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
Gigabyte
TotalGB
Shows the total memory space. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
Gigabyte
Network
AdapterName
Shows the network adapter name. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Text
N/A
IPv4
Shows the IPv4 address. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Text
N/A
IPv6
Shows the IPv6 address. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Text
N/A
ReceiveKbps
Shows the average number of bytes per second received by the process in the last minute. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
Kilobyte per second
SendKbps
Shows the average number of bytes per second sent by the process in the last minute. This attribute is retrieved from Windows and can be viewed on the Task Manager’s
Performance
tab.
Numeric
Kilobyte per second
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal