FactoryTalk Alarms and Events Database Update Utility

Use the
FactoryTalk
Alarms and Events Database Update Utility to update the database by:
  • Merging the ConditionEvent and TrackingEvent tables into the AllEvent table in the same database.
  • Creating the AllEvent, Diagnostic, or Messages table if any of them doesn't exist.
  • Associating the vmAllEvents view with the AllEvent table.
For earlier versions of
FactoryTalk Alarms and Events
, the response time of
FactoryTalk
Alarm and Event Log Viewer may be very slow. Because it needs to extract historical data from more than one tables (ConditionEvent and TrackingEvent), especially when the tables contain a large volume of data.
Starting from
FactoryTalk Alarms and Events
version 2.90.00 (CPR 9 SR 9), when
FactoryTalk
Alarm and Event Historian logs historical alarm and event data into a database in
Microsoft®
SQL Server®
, an additional table, AllEvent, is created. Starting from
FactoryTalk Alarms and Events
version 6.20.00 (CPR 9 SR 12), ConditionEvent and TrackingEvent tables are no longer created. This data is only logged into the AllEvent table. As a result, by extracting historical data from the AllEvent table, the response time of
FactoryTalk
Alarm and Event Log Viewer is optimized.
By updating the database, the
FactoryTalk Alarms and Events
Database Update Utility merges the ConditionEvent and TrackingEvent tables included in the historical alarm and event database from earlier versions of
FactoryTalk Alarms and Events
into the AllEvent table. All the data in the AllEvent table is queried by
FactoryTalk
Alarm and Event Log Viewer.
If the database is created from earlier versions of
FactoryTalk Alarms and Events
, the AllEvent, Diagnostic, or Messages table may not exist depending on the database schema of that version. Updating the database also creates any of the tables in the database if they don't exist.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal