Items in the Database Update Utility window

The following table lists the items and their meanings in the
FactoryTalk Alarms and Events
Database Update Utility window.
Items
Description
Database list
The list of historical alarm and event databases in the currently connected
Microsoft
SQL Server
.
Message list
Messages of database update operations, including the
SQL Server
version, the utility behaviors, and error information.
Server name
The server name of the currently connected
SQL Server
.
Database name
The currently selected historical alarm and event database.
Duration
The time used for the database update process.
Process
The progress bar of the database update process.
Migrate
Click the button to start the database update process.
Cancel
Click the button to cancel the database update process.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal