Process tab

The following are the settings on the
Process
tab of the
FactoryTalk Resource and Status
Server Properties
dialog. It shows when
Enable data from workstation and processed monitoring
is selected.
Setting
Description
Add
Opens the
Add Process
dialog to add processes that you want to monitor.
Delete
Deletes the processes that you select.
Export
Exports the process list as a CSV file.
Import
Imports a CSV file that contains the process list.
Process Name
Shows the name of the processes that you want to monitor.
Alias Name
Enters the alias name processes. It is optional.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal