Delete a process

Delete one or multiple processes once you don't want to monitor.
To delete a process
  1. On the
    Process
    tab, select the processes that you want to delete.
  2. Select
    Delete
    .
    Select
    Yes
    when the
    Confirm
    dialog prompts
  3. Select
    Apply
    to save the changes.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal