Device Status tab

Frequent updates for a high number of addresses may cause network congestion. The following are the settings on the
Device Status
tab.
Setting
Description
Number of addresses to ping as a group
Configures the device quantity in a group to ping simultaneously.
Interval between each ping group (seconds)
Sets the time interval between each ping group.
Interval between each complete cycle group (seconds)
Sets the time interval between each data collection cycle of all devices.
New
Adds one or multiple device addresses manually.
Delete
Deletes one or multiple device addresses.
Export
Exports the device address list as a CSV file.
Import
Imports a CSV file that contains the device address list.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal