Add a process

Add one or multiple processes running on the computer hosing the FactoryTalk Resource and Status server to monitor.
To add a process
  1. On the
    Process
    tab, select
    Add
    .
  2. In the
    Add Process
    dialog, select a method to add a process.
    • Add from Task Manager
      It is only available for the local host.
      Select one or multiple processes, and then select
      OK
      . Use the
      Refresh
      function to get the latest data and the
      Search
      function to find the desired process.
    • Add by process name
      Select
      New
      , enter the process name that you want to monitor, and then select
      OK
      .
  3. Select
    Apply
    to save the changes.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal