Add a device address

Add one or multiple device addresses that you want to monitor.
To add a device address
  1. On the
    Device Status
    tab, select
    New
    .
  2. Enter a device address that you want to monitor, such as IPv4, hostname, or DNS.
    The alias name is optional.
  3. Select
    Apply
    to save the changes.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal