Delete a device address

Delete one or multiple device addresses when you don't want to monitor.
  1. On the
    Device Status
    tab, select the device addresses that you want to delete.
  2. Select
    Delete
    .
    Select
    Yes
    when the
    Confirm
    dialog prompts.
  3. Select
    Apply
    to save the changes.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal