Breadcrumb navigation

Use these methods to navigate a hierarchy through breadcrumbs.
To do this:
Do this:
Access a level.
Click any level except the last.
Return to the highest level of the hierarchy.
Click
Home
Home icon.
Open a list of sub-levels.
Click the single arrow Single arrow. Select a level from the list.
Return to a recently navigated path.
Click the double arrow Right double arrow or Left double arrow to open a list of links.
小贴士:
If a breadcrumb is too long to fit in the window, the window displays a double arrow. A double arrow indicates there is more content to the left or to the right of the current location in the breadcrumb.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal