FactoryTalk Linx Network Browser

How do I open the
FactoryTalk Linx
Network Browser?
From a
Rockwell Automation
software application, click the
Network Browser
Network Browser icon to launch the
Network Browser
.
The
FactoryTalk Linx
Network Browser
is an interactive
FactoryTalk Linx
Network Browser included with
Rockwell Automation
software applications that is used to navigate network topologies and configure the access methods used by applications to communicate with devices.
It creates and modifies device networking configurations. It shares networking configuration with
FactoryTalk Linx
in the
FactoryTalk Administration Console
.
Log on to
FactoryTalk Diagnostics
before configuring the
FactoryTalk Linx
Browser, or the
FactoryTalk Linx
Network Browser operates under Read-only mode.
Use the
FactoryTalk Linx
Network Browser
dialog box to:
  • Navigate a network topology to locate a device for interaction
  • Automatically discover devices
  • Add and delete drivers
  • Edit driver settings
  • Search for devices
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal