Reroot a view

Reroot a view in the
FactoryTalk Linx
Network Browser
network topology tree to limit the view to a selected area in the topology.
To reroot a view
  1. In the network topology tree in the
    FactoryTalk Linx
    Network Browser
    , select a node in the tree. The anchor appears.
  2. Click the anchor Anchor icon icon to make the selected row into the new root.
    In the breadcrumbs area, an anchor icon appears next to the item within the topology where it is anchored.
  3. Click the anchor icon again to return to the normal view.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal