Refresh a device or network display

Clicking
Refresh
instructs the
FactoryTalk Linx
Network Browser
to perform one discovery cycle of the selected device or network. Since
Refresh
only performs one discovery cycle, clicking
Refresh
multiple times might be necessary to discover everything on the network and display them in the
FactoryTalk Linx
Network Browser
.
To refresh a device or network display
  1. In the
    FactoryTalk Linx
    Network Browser
    dialog box, click the device or network to refresh the network topology tree display.
  2. Click
    Refresh
    Refresh icon. The icon next to the selected device or network animates to indicate a discover cycle is being performed.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal