CIP Security tab

Select the
CIP Security
tab to view and edit the CIP Security settings of a device:
Setting
Description
Network Port
Used to display the port label assigned by the manufacturer.
This item cannot be edited. It displays a label that is corresponding to a given port. This label is obtained directly from the device. In case where it was impossible to obtain the label from the device, the label will be set to "1". Updating the device’s firmware, if the label displayed is incorrect.
CIP Security Configuration Status
Shows the CIP security configuration status of devices.
Configured
Means the device is configured to utilize CIP security with
FactoryTalk Policy Manager
.
Not Configured (Factory Default)
Means the device's CIP security configuration is cleared. All security settings are now in Factory Default mode (CIP Security not active but can be configured if the CIP Security port is enabled). Note the CIP Security port 2221 is open when the device is in this state.
In Progress
The configuration of CIP Security is in progress.
Incomplete configuration
The configuration of CIP Security is not completed yet.
Unknown
There was an unknown error in retrieving the value of the status.
UDP/TCP Port 2221 Status
Shows the status of 2221 IANA Port.
Enabled
Port 2221 is enabled.
Disabled
Port 2221 is disabled, and it can only be re-enabled by resetting the device to its factory default configuration.
Pending
This device has a pending port change and requires a reset.
Unknown
There was an unknown error in retrieving the value of the status.
Disable CIP Security (Port 2221)
Select this checkbox to disable port 2221 for both TCP and UDP communications.
These ports are used for CIP Security communication. CIP Security cannot be used if these ports are disabled. The change will be committed after
Apply
button is pressed.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal