Locate a device

If a device is not in the
FactoryTalk Linx
Network Browser
network topology tree, perform the following tasks:
  • Perform a search for the device
  • Add a driver
  • Copy and paste items into a driver
    小贴士:
    Make sure the
    FactoryTalk Linx
    Network Browser has created a cache of information for a device prior to performing a search.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal