Delete drivers

Delete drivers if they are no longer in use.
To delete drivers
To delete drivers, do one of the following:
  • In the
    FactoryTalk Linx
    Network Browser
    dialog box, select a driver, right-click the driver and select
    Delete
    .
  • In the
    FactoryTalk Linx
    Network Browser
    dialog box, select Configure Drivers, select a single or multiple drivers, and then select
    Delete
    .
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal