Configure Driver dialog

How do I open the Configure Driver dialog?
  1. From the
    Network Browser
    tree, click the driver.
  2. Click the
    Property
    icon.
Use the
Configure Driver
dialog to:
  • Modify the name of the driver
  • Adjust the Discovery Method
    • Change broadcast settings
    • Modify the list of device addresses in a
      Device List/Range
    • Edit an item to a list in a driver
    • Adjust the advanced network speed of browsing settings
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal