Auto discover a device or network

The Auto discover function enables the
FactoryTalk Linx
Network Browser
to continuously scan a selected device or network and provide real-time status updates. For example, if Auto discover is enabled, the
FactoryTalk Linx
Network Browser
recognizes nodes during the discover cycle and stores the node information. If an error occurs, such as a communication cable being pulled from a device, the
FactoryTalk Linx
Network Browser
places a red X over the device to indicate that it cannot be recognized.
The selection does not have to be expanded to enable Auto discover function to execute.
To Auto discover a selected device or network
  1. In the
    FactoryTalk Linx
    Network Browser
    dialog box, click a device or network to auto discover in the network topology tree.
  2. Click
    Auto discover
    Auto discover. The icon next to the selected device or network animates to indicate auto discovery.
  3. To stop auto browsing the device or network, click
    Auto discover
    Auto discover again.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal