示例:SelectedPenScale 属性

Private Sub SelectNextPen_Click() Dim nPen As Integer Dim nAttempt As Integer 'Jump to end of subroutine If Trend1.Pens.Count = 0 Then Exit Sub End If 'get the currently selected pen nPen = Trend1.YAxis.SelectedPenScale For nAttempt = 0 To Trendx1.Pens.Count nPen = nPen + 1 If nPen > Trendx1.Pens.Count Then nPen = 1 End If 'only select a visible pen If Trend1.Pens.Item(nPen).Visible Then Trend1.YAxis.SelectedPenScale = nPen Exit For End If Next End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal