示例:Name 属性

Private Sub GetTagsInModel() Dim s As String Dim p As Pen ' Go through all Pens in the collection For Each p In TrendX1.Pens ' Find the Pens that are in the CureProc data log model If p.DataLogModelName = "CureProc" Then s = s & ", " & p.Name End If Next MsgBox "Pens from the CureProc Data Log Model: " & s End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal