示例:Error 属性

Private Sub CheckPenError(PenNumber As Integer) If Trend1.Pens(PenNumber).Error = True Then MsgBox "Tag is in error. Make sure it is communicating properly." Else MsgBox "Tag value is valid." End If End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal