示例:Color 属性

Private Sub SetLineGreen() Dim s As String Dim p As Pen ' Notice that the pen numbers are 1-based ' Pen(1) is the first pen, not Pen(0) Set p = Trend1.Pens(1) s = "The " & p.Description & " line was color #" & p.Color MsgBox s, vbOKOnly p.Color = rstColorGreen End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal