示例:Upper/LowerBoundPenIndex 属性

Private Sub SetShading() ' For this example to work, trend must not have any pens previously added Trend1.Pens.Add "TankLevel", "", "", 0, 100 Trend1.Pens.Add "25", "Low Alarm", "", 0, 100 Trend1.Pens.Add "75", "High Alarm", "", 0, 100 Trend1.Pens.Item(1).LowerBoundPenIndex = 2 Trend1.Pens.Item(1).UpperBoundPenIndex = 3 End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal