FactoryTalk Resource and Status server backup and restore

The FactoryTalk Resource and Status server backup and restore is along with the FactoryTalk Directory. Once the FactoryTalk Resource and Status server is restored, you need to update the server computer name if the server computer is changed.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal