Feature security properties

The following table shows the relationship between FactoryTalk Resource and Status feature security policies and securable actions that the user can perform:
Feature security policy
Allow
Deny
View Configurations
Allow users to view the FactoryTalk Resource and Status server configurations.
Hide the FactoryTalk Resource and Status server configurations.
Modify Configurations
Allow users to edit the FactoryTalk Resource and Status server configurations.
Set the FactoryTalk Resource and Status server configurations as read-only.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal