Redundant Adapter Pair mode displays

The
Network Browser
supports browsing and configuring 5015 and 1756-EN4TR adapters in Redundant Adapter Pair (RAP) mode. The redundant adapters will be automatically listed together in the
Network Browser
at the location determined by the lowest IP address. The I/O modules in a chassis under these adapters are also automatically grouped when they are redundant pair. The RAP icon icon indicates the I/O modules are redundant pair.
In this mode, if one of the adapters or I/O modules is offline, Offline devices icon icon appears on the left, indicating the device's offline status.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal