Offline devices

Starting from
FactoryTalk Linx
version 6.30, the offline devices will be shown. The Offline devices icon icon to the left of the device indicates this device is offline.
To remove one offline device, right-click the device, and then select
Delete
.
To remove the current offline devices listed in the driver, right-click the driver, and then select
Remove Offline Devices
.
To remove offline devices automatically every time after browsing devices, right-click the driver, and then select
Driver Configuration
>
Advanced
>
Tuning
>
Auto remove offline devices.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal