LLDP tab

Select the
LLDP
tab to view and edit the Link Layer Discovery Protocol (LLDP) settings and access information from connected devices. LLDP is a low level Ethernet protocol used to identify external devices connected to each device’s network interface connection. The Open Vendors Device Association (ODVA) incorporated LLDP into the Common Industrial Protocol (CIP) and expanded it to include CIP device identity information to enhance the ability to identify CIP devices connected in an automation system. This tab is only available for devices that support LLDP detection.
Setting
Description
Global Configuration and Information
Global LLDP Status
Shows the status of LLDP detection in this device. Select
Enabled
to turn on the LLDP detection. Unselect
Enabled
to turn it off.
LLDP Datastore
Shows the retrieval methods for the LLDP database supported by the device, including:
  • LLDP Data Table Object
  • SNMP
  • NETCONF YANG
  • RESTCONF YANG
Parameter Configuration
Transmit Interval
Shows the interval in seconds at which LLDP frames are transmitted from this device.
Hold Multiplier
Shows a multiplier of
Transmit Interval
to determine the value sent to neighbor devices.
Port Configuration and Device Connected
Port
Shows the port name of this device.
Outgoing Enabled
Indicates whether this port is enabled to send information.
If this port is enabled, it is used to send this device's information to the neighbor device and receive information from the neighbor device. If this port is disabled, this device only receives the neighbor device information through this port.
Neighbor Information
Shows the information for the devices connected to each port of this device, including:
  • IP Address
  • Port
  • Device Name
  • Revision
  • MAC Address
  • Vendor
小贴士:
Select LLDP copy table icon to copy the
Port Configuration and Device Connected
table.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal