FactoryTalk Linx Redundancy Module Configuration Tool

FactoryTalk Linx
Redundancy Module Configuration Tool is a separately installed tool opened within the
FactoryTalk Linx
Network Browser to permit online operations and configuration of a
ControlLogix
redundancy modules.
FactoryTalk Linx
Redundancy Module Configuration Tool uses FactoryTalk audit logging and creates audit messages for each action performed on the redundancy module. In addition, it shows the current chassis label, redundancy status, and chassis platform configuration in the lower-left corner of the dialog and updates the status every two seconds.
FactoryTalk Linx
Redundancy Module Configuration Tool version 9.01.01 is installed along with
FactoryTalk Linx
version 6.21.00 or later by default. You can also get the tool from the Product Compatibility and Download Center. It is compatible with
FactoryTalk Linx
version 6.21.00 or later and supports 1756-RM2 modules with firmware version 20.010 or later.
FactoryTalk Linx
Redundancy Module Configuration Tool version 10.01.00 can be obtained from Product Compatibility and Download Center. It is compatible with FactoryTalk Linx version 6.60.00 and supports the 1756-RM2 modules, like the version 9.01.01, but adds support for 1756-RM3 modules.
You can configure FactoryTalk Security to grant
Open Device Configuration
to access FactoryTalk Linx Redundancy Module Configuration Tool. Otherwise,
FactoryTalk Linx
Network Browser will not allow the tool to open.
小贴士:
In
FactoryTalk Administration Console
, go to
System > Policies > Product Policies >
FactoryTalk Linx
> Feature Security
to set the
Open Device Configuration
permission.
To open the tool, locate a 1756-RM2 redundancy module in the
FactoryTalk Linx
Network Browser topology view, right-click the module, and then select
Device Configuration
. If version 10.00.00 of the tool is installed, you can also locate a 1756-RM3 redundancy module in the topology view and perform the same actions.
For more information, see the
FactoryTalk Linx
Redundancy Module Configuration Tool Help
.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal