创建 UIPopulator NetLogic

创建用于根据模型对象属性自动创建 UI 元素的 NetLogic。
先决条件
设置默认外部代码编辑器。请参见设置默认代码编辑器。
  1. 创建 UIPopulator NetLogic
  2. 在
    项目视图
    中,右键单击
    垂直布局1
    ,然后选择
    新建
    运行时 NetLogic
    。
  3. 将光标悬停在 NetLogic 上,选择
    编辑图标
    并输入
    UIPopulator
    。
  4. 双击 NetLogic。
    外部代码编辑器将打开。
  5. 在代码编辑器中,使用以下代码替换现有代码:
    using System.Linq; using FTOptix.HMIProject; using FTOptix.UI; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; public class UIPopulator : FTOptix.NetLogic.BaseNetLogic { public override void Start() { // Get the Model variable of the ListBox modelObjectVariable = LogicObject.Get<IUAVariable>("ModelObject"); // Subscribe to the VariableChange event modelObjectVariable.VariableChange += ModelObjectVariable_VariableChange; // Build the UI based on the selected item BuildUI(modelObjectVariable.Value); } private void ModelObjectVariable_VariableChange(object sender, VariableChangeEventArgs e) { // Every time the ModelObject variable changes, rebuild the UI BuildUI(e.NewValue); } public override void Stop() { // Destroy the variable change event modelObjectVariable.VariableChange -= ModelObjectVariable_VariableChange; } private void BuildUI(NodeId modelObjectNodeId) { // Get the VerticalContainer that will hold the UI elements var verticalContainer = (ColumnLayout)Owner; // Get the ModelObject of the VerticalLayout from the NodeId var modelObject = InformationModel.Get(modelObjectNodeId); // Clear all the children of the VerticalContainer foreach (var child in verticalContainer.Children.OfType<Item>()) { child.Delete(); } // Create the UI elements based on the DataType of the children of the ModelObject foreach (var objectProperty in modelObject.Children.OfType<IUAVariable>()) { Item uiObject; if (objectProperty.DataType == OpcUa.DataTypes.Boolean) uiObject = MakeSwitch(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.String) uiObject = MakeTextBox(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.Int32) uiObject = MakeLinearGauge(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.Float) uiObject = MakeCircularGauge(objectProperty); else if (objectProperty.DataType == FTOptix.Core.DataTypes.ResourceUri) uiObject = MakeImage(objectProperty); else uiObject = MakeTextBox(objectProperty); // Add the UI element to the VerticalContainer if (uiObject != null) verticalContainer.Add(uiObject); } } private static Panel MakeBaseContainer(IUAVariable variable) { // Create a Panel to hold the UI element var container = InformationModel.MakeObject<Panel>("ControlContainer"); container.Height = 50; container.HorizontalAlignment = HorizontalAlignment.Stretch; // Create a Label to show the name of the variable var label = InformationModel.MakeObject<Label>("Label"); label.VerticalAlignment = VerticalAlignment.Center; label.LeftMargin = 20; label.Text = variable.BrowseName; // Add the Label to the Panel container.Add(label); return container; } private static Item MakeSwitch(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); var mySwitch = InformationModel.MakeObject<Switch>("Switch"); mySwitch.HorizontalAlignment = HorizontalAlignment.Right; mySwitch.VerticalAlignment = VerticalAlignment.Center; mySwitch.RightMargin = 40; // Bind the Checked property of the Switch to the variable MakeDataBind(mySwitch.Children.Get<IUAVariable>("Checked"), variable); // Add the Switch to the container container.Add(mySwitch); return container; } private static Item MakeTextBox(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); var textBox = InformationModel.MakeObject<TextBox>("TextBox"); textBox.HorizontalAlignment = HorizontalAlignment.Right; textBox.VerticalAlignment = VerticalAlignment.Center; textBox.RightMargin = 40; // Bind the Text property of the TextBox to the variable MakeDataBind(textBox.Children.Get<IUAVariable>("Text"), variable); // Add the TextBox to the container container.Add(textBox); return container; } private static Item MakeCircularGauge(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); container.Height = 180; // Create a CircularGauge var circularGauge = InformationModel.MakeObject<CircularGauge>("CircularGauge"); circularGauge.Width = 140; circularGauge.HorizontalAlignment = HorizontalAlignment.Right; circularGauge.VerticalAlignment = VerticalAlignment.Stretch; circularGauge.RightMargin = 40; circularGauge.TopMargin = 20; // Bind the Value property of the CircularGauge to the variable MakeDataBind(circularGauge.Children.Get<IUAVariable>("Value"), variable); // Add the CircularGauge to the container container.Add(circularGauge); return container; } private static Item MakeLinearGauge(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); container.Height = 150; // Create a LinearGauge var linearGauge = InformationModel.MakeObject<LinearGauge>("LinearGauge"); linearGauge.Width = 140; linearGauge.Height = 35; linearGauge.HorizontalAlignment = HorizontalAlignment.Right; linearGauge.VerticalAlignment = VerticalAlignment.Center; linearGauge.RightMargin = 40; linearGauge.TopMargin = 20; // Bind the Value property of the LinearGauge to the variable MakeDataBind(linearGauge.Children.Get<IUAVariable>("Value"), variable); // Add the LinearGauge to the container container.Add(linearGauge); return container; } private static Item MakeImage(IUAVariable variable) { // Create the image object var image = InformationModel.MakeObject<Image>("Image"); image.HorizontalAlignment = HorizontalAlignment.Center; image.Width = 100; image.Height = 100; image.TopMargin = 20; image.BottomMargin = 20; // Set the path property of the image object image.Path = new FTOptix.Core.ResourceUri(variable.Value); return image; } private static void MakeDataBind(IUAVariable property, IUAVariable targetVariable) { // Set the DynamicLink to a variable as ReadWrite property.SetDynamicLink(targetVariable, FTOptix.CoreBase.DynamicLinkMode.ReadWrite); } private IUAVariable modelObjectVariable; }
  6. 保存代码。
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal