创建 UIPopulator NetLogic

创建用于根据模型对象属性自动创建 UI 元素的 NetLogic。
先决条件
设置默认外部代码编辑器。请参见设置默认代码编辑器
  1. 创建 UIPopulator NetLogic
  2. 项目视图
    中,右键单击
    垂直布局1
    ,然后选择
    新建
    运行时 NetLogic
  3. 将光标悬停在 NetLogic 上,选择
    Edit
    并输入
    UIPopulator
  4. 双击 NetLogic。
    外部代码编辑器将打开。
  5. 在代码编辑器中,使用以下代码替换现有代码:
    using System.Linq; using FTOptix.HMIProject; using FTOptix.UI; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; public class UIPopulator : FTOptix.NetLogic.BaseNetLogic { public override void Start() { // Get the Model variable of the ListBox modelObjectVariable = LogicObject.Get<IUAVariable>("ModelObject"); // Subscribe to the VariableChange event modelObjectVariable.VariableChange += ModelObjectVariable_VariableChange; // Build the UI based on the selected item BuildUI(modelObjectVariable.Value); } private void ModelObjectVariable_VariableChange(object sender, VariableChangeEventArgs e) { // Every time the ModelObject variable changes, rebuild the UI BuildUI(e.NewValue); } public override void Stop() { // Destroy the variable change event modelObjectVariable.VariableChange -= ModelObjectVariable_VariableChange; } private void BuildUI(NodeId modelObjectNodeId) { // Get the VerticalContainer that will hold the UI elements var verticalContainer = (ColumnLayout)Owner; // Get the ModelObject of the VerticalLayout from the NodeId var modelObject = InformationModel.Get(modelObjectNodeId); // Clear all the children of the VerticalContainer foreach (var child in verticalContainer.Children.OfType<Item>()) { child.Delete(); } // Create the UI elements based on the DataType of the children of the ModelObject foreach (var objectProperty in modelObject.Children.OfType<IUAVariable>()) { Item uiObject; if (objectProperty.DataType == OpcUa.DataTypes.Boolean) uiObject = MakeSwitch(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.String) uiObject = MakeTextBox(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.Int32) uiObject = MakeLinearGauge(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.Float) uiObject = MakeCircularGauge(objectProperty); else if (objectProperty.DataType == FTOptix.Core.DataTypes.ResourceUri) uiObject = MakeImage(objectProperty); else uiObject = MakeTextBox(objectProperty); // Add the UI element to the VerticalContainer if (uiObject != null) verticalContainer.Add(uiObject); } } private static Panel MakeBaseContainer(IUAVariable variable) { // Create a Panel to hold the UI element var container = InformationModel.MakeObject<Panel>("ControlContainer"); container.Height = 50; container.HorizontalAlignment = HorizontalAlignment.Stretch; // Create a Label to show the name of the variable var label = InformationModel.MakeObject<Label>("Label"); label.VerticalAlignment = VerticalAlignment.Center; label.LeftMargin = 20; label.Text = variable.BrowseName; // Add the Label to the Panel container.Add(label); return container; } private static Item MakeSwitch(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); var mySwitch = InformationModel.MakeObject<Switch>("Switch"); mySwitch.HorizontalAlignment = HorizontalAlignment.Right; mySwitch.VerticalAlignment = VerticalAlignment.Center; mySwitch.RightMargin = 40; // Bind the Checked property of the Switch to the variable MakeDataBind(mySwitch.Children.Get<IUAVariable>("Checked"), variable); // Add the Switch to the container container.Add(mySwitch); return container; } private static Item MakeTextBox(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); var textBox = InformationModel.MakeObject<TextBox>("TextBox"); textBox.HorizontalAlignment = HorizontalAlignment.Right; textBox.VerticalAlignment = VerticalAlignment.Center; textBox.RightMargin = 40; // Bind the Text property of the TextBox to the variable MakeDataBind(textBox.Children.Get<IUAVariable>("Text"), variable); // Add the TextBox to the container container.Add(textBox); return container; } private static Item MakeCircularGauge(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); container.Height = 180; // Create a CircularGauge var circularGauge = InformationModel.MakeObject<CircularGauge>("CircularGauge"); circularGauge.Width = 140; circularGauge.HorizontalAlignment = HorizontalAlignment.Right; circularGauge.VerticalAlignment = VerticalAlignment.Stretch; circularGauge.RightMargin = 40; circularGauge.TopMargin = 20; // Bind the Value property of the CircularGauge to the variable MakeDataBind(circularGauge.Children.Get<IUAVariable>("Value"), variable); // Add the CircularGauge to the container container.Add(circularGauge); return container; } private static Item MakeLinearGauge(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); container.Height = 150; // Create a LinearGauge var linearGauge = InformationModel.MakeObject<LinearGauge>("LinearGauge"); linearGauge.Width = 140; linearGauge.Height = 35; linearGauge.HorizontalAlignment = HorizontalAlignment.Right; linearGauge.VerticalAlignment = VerticalAlignment.Center; linearGauge.RightMargin = 40; linearGauge.TopMargin = 20; // Bind the Value property of the LinearGauge to the variable MakeDataBind(linearGauge.Children.Get<IUAVariable>("Value"), variable); // Add the LinearGauge to the container container.Add(linearGauge); return container; } private static Item MakeImage(IUAVariable variable) { // Create the image object var image = InformationModel.MakeObject<Image>("Image"); image.HorizontalAlignment = HorizontalAlignment.Center; image.Width = 100; image.Height = 100; image.TopMargin = 20; image.BottomMargin = 20; // Set the path property of the image object image.Path = new FTOptix.Core.ResourceUri(variable.Value); return image; } private static void MakeDataBind(IUAVariable property, IUAVariable targetVariable) { // Set the DynamicLink to a variable as ReadWrite property.SetDynamicLink(targetVariable, FTOptix.CoreBase.DynamicLinkMode.ReadWrite); } private IUAVariable modelObjectVariable; }
  6. 保存代码。
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈
Normal