Loading
Overview

Academy of Advanced Manufacturing IACT Certification Skill List

分享:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

Graduates of the Academy of Advanced Manufacturing will be certified by Rockwell Automation to be capable of successful execution of the following:

  • Interpreting wiring diagrams used in an Industrial Automation and Control System (IACS)
  • Describing, understanding, and troubleshooting the various factory floor electro-mechanical components in an IACS such as fuses, relays, contactors, digital and analog inputs and outputs and common instrumentation devices
  • Operate, support and troubleshoot small and medium-scope Programmable Logic Controllers, and supporting projects associated with those controllers
  • Troubleshooting ladder-logic based Programmable Logic Controllers
  • Designing, programming, and troubleshooting plant floor Human Machine Interfaces (HMI)
  • Tracing operationl data from plant floor electro-mechanical devices to the controller, HMI within an IACS
  • Performing a preventive maintenance schedule on plant floor equipment
  • Starting-up, maintaining, and troubleshooting low voltage variable frequency drives, with power ranging from 1 HP to 300+ HP
  • Troubleshooting layer 1 and layer 2 networking components within an industrial Ethernet environment

(IACT = Instrumentation & Automation Control Technician)

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation 主页
  2. Chevron LeftChevron Left 支持
  3. Chevron LeftChevron Left 文档
  4. Chevron LeftChevron Left Academy of Advanced Manufacturing IACT Certification Skill List