Loading
Case Study | Healthcare and Logistics
Recent ActivityRecent Activity

Public Health Emergency Response Simulation

Arena® Simulation Software improves efficiency in deploying emergency response services during a crisis.

分享:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Doctor reviewing virtual skeleton

Challenge

To quantify and validate tangible aspects of emergency preparedness and response.

Solutions

An Arena Simulation was built to include the steps upon receiving a request for emergency services and the deployment to these areas.

Results

Based on analysis, investments in lab capacity would have the most significant impact on the performance and capacity of NC PHIN during a state-wide E.coli outbreak. We determined this by identifying the resource that was limiting the overall capacity of NC PHIN based on queue wait times and resource utilization. The findings from the simulation also highlight the fact that the existence of capacity doesn’t imply that the capacity is being fully utilized. Bottlenecks in the upstream stages of a process limit the utilization (and realized capacity) of subsequent resources.

Background

The attacks of September 11th, the 2005 Indian Ocean Tsunami and the recent Swine Flu Outbreak have all highlighted the need for more resilient and responsive public health infrastructures. Following the attacks of September 11th, a growing fear of a bioterrorist attack emerged within the United States and pushed the threat of bioterrorism to the forefront of the public health emergency preparedness and response agenda.(Association of Schools of Public Health 2004) As a result, an influx of funding to support the development of many public health emergency preparedness and response systems was provided to improve public health infrastructures. Given the sense of urgency that surrounded the development of many of these systems, very little oversight and detail was provided to determine how the efficacy of these systems would be governed, measured and evaluated. Despite the investment of more than six billion dollars towards public health emergency preparedness and response initiatives since 2001, many would agree that valid, well defined and broadly accepted performance measures have yet to be established.

Challenge

The goal is to present a methodology for capturing the value of emergency preparedness and response systems, such as NC PHIN. Ultimately we seek to answer the following question: How has NC PHIN increased emergency preparedness and response capacity with respect to the ability to efficiently prepare for and respond to events that involve communicable diseases? In seeking to answer this question a simulation model was developed of the 2004 North Carolina State Fair E.coli Outbreak to quantitatively capture the capacity of the less tangible aspects of emergency preparedness and response systems.

Solution

Due to the complexity of public health emergency response, prior to building our simulation model we narrowed the focus of our analysis down to a specific threat. The 2004 State Fair E.coli Outbreak was selected as a representative communicable disease outbreak in North Carolina.(Goode and O’Reilly 2005) The 2004 State Fair E.coli Outbreak case was selected for the following reasons:

  • This event was one of the largest petting zoo outbreaks of E.coli to date.
  • It was a statewide public health threat. Statewide events require communication across jurisdictions and organizations, which was an area we were interested in analyzing.
  • The state fair attracted visitors from a variety of counties, providing the opportunity to observe the variability in response among the different counties.

 

Results

In the analysis of the NC PHIN system, primary areas of improvement are identified by potential bottlenecks in our system. As explained earlier, long queue times in a process followed by significantly shorter queue times in subsequent stages of the process are used to identify bottlenecks in the system. For this analysis the average queue waiting times provided insight into potential system bottlenecks. As indicated by Table 1, our data implies that the bottleneck in NC PHIN is primarily associated with the lab capacity. This is suggested by the long wait times in queue for the lab resource followed by subsequent processes with no queues. Furthermore, the lower utilization of other resources in the system indicate that the NC PHIN system has some level of capacity that is not being utilized which further supports our hypothesis that the lab may be the source of NCPHIN’s bottleneck, limiting the effectiveness of other resources.

Our findings suggest that investments in improving overall system performance of NC PHIN should be aimed at improving lab capacity. Although other capacities may still be important, investing in priorities other than the bottleneck may not provide as much of a return on the investment in the overall system performance if the value of competing priorities are being limited by the bottleneck. Therefore, from an economic standpoint, since lab capacity is the resource that is constraining our 1964 Wynter and Ivy system’s capacity, it should be the primary area of focus in establishing investment priorities (e.g. funding or the allocation of resources) for improving the performance of the public health response system (NC PHIN). 

发布时间 2014年8月1日

Download the Whitepaper
主题: Arena Simulation Software Healthcare Simulation Software Logistics Simulation Software

准备好下单您的软件了吗?

订单选项
Software SubscriptionsSoftware Subscriptions
订单选项

一站式购买软件和订阅服务。

浏览我们的订单选项
与顾问探讨
DistributorDistributor
与顾问探讨

与您当地的 Rockwell Automation 销售顾问合作,以探讨您的软件要求。

联系我们

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation 主页
  2. Chevron LeftChevron Left 产品
  3. Chevron LeftChevron Left 软件
  4. Chevron LeftChevron Left Arena 仿真软件
  5. Chevron LeftChevron Left Arena Simulation Software Case Studies
  6. Chevron LeftChevron Left Public Health Emergency Response Simulation