Loading
Case Study | Government & Military
Recent ActivityRecent Activity

Improve Personnel Training Procedures

Arena® Simulation Software helps determine the best amount of people to move through different stages of training.

分享:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
silhouette of solider saluting against sunrise

Challenge

Sustain up to three expeditionary operations, simultaneously, in potentially three different theatres of operation.

Solutions

Arena Simulation was built to review the different stages and time it takes to move through the various sections and ensure positions could be filled.

Results

The concept model built shows projections for shortages in various positions. This allows for planning to train and fill these positions to avoid absences.

Background

This paper presents a proof-of-concept discrete-event simulation model for examining the ability of the Canadian Forces (CF) to sustain operations, from a human resources perspective. Given a set of future operations for the CF, ranging from known ongoing domestic commitments to possible international missions, the goal is to identify potential shortages of deployable personnel by occupation, rank and unit, up to five years in advance of actual deployment. As a demonstration case, the proof-of-concept model was applied to a contingency analysis of the sustainability of Task Force Afghanistan over a three year planning horizon.

Challenge

The Government of Canada’s Defense Policy Statement delineated a series of future tasks for the Canadian Forces (CF) in support of Canada’s role in contributing to international peace and stability. Included in the list of specific tasks are: the ability to sustain for an indefinite period of time two land-based Mission Specific Task Forces of approximately 1,200 personnel each, in potentially different theatres of operation; and the ability to deploy a third task force of approximately 1,000 personnel for up to six months either to reinforce a current operation or mount a new short-term mission.

Solution

When running the operational sustainability model, there are two options: to restrict the pool of nominees to those in deployable units (the model default), or to allow all deployable members regardless of their unit type to be eligible for selection. The aim of running the model is to identify potential shortages of positions (and by association personnel) in the CF establishment by unit, occupation and rank. The shortages identified in the model can be of two types: the position was filled but an operational waiver had to be signed, or the position could not be filled at all. In the latter case this can be due to: there not being any personnel in the pool of potential nominees with the requisite characteristics (correct occupation and rank); or all personnel with the requisite characteristics were already deployed or in a mandatory 60 day respite period. 

Results

In this paper, we have presented a proof-of-concept model for assessing the ability of the CF to sustain operations. The operational sustainability model can provide projections of potential personnel shortages several years in advance of deployments, and enables the assessment of whether or not the distribution of deployable versus nondeployable positions across the CF is appropriate for meeting operational demands. This study shows one way in which modeling and simulation can be used to inform the operational planning process, and the generation (assembly, training and deployment) of forces to meet the requirement.

The application of the proof-of-concept model to the analysis of sustaining TFA provided insight into several improvements that should be made to the model, in order to provide a more holistic and realistic analysis of the CF’s ability to meet operational demands. In future phases of the project, the model logic will be enhanced to determine Reserve Force augmentation patterns stochastically based on historical rates, rather than the current hard-coding of specific positions. Linkages to existing models for projecting demographic changes should also be incorporated so the input population can be updated annually within the model to reflect the effects of attrition, promotions, postings and recruitment on the deployable population. As well, future versions of the model should incorporate both stochastic and deterministic mechanisms for deciding when future tasks and operations will occur.

发布时间 2014年8月1日

Download the Whitepaper
主题: Arena Simulation Software Government and Military Simulation Software

准备好下单您的软件了吗?

订单选项
Software SubscriptionsSoftware Subscriptions
订单选项

一站式购买软件和订阅服务。

浏览我们的订单选项
与顾问探讨
DistributorDistributor
与顾问探讨

与您当地的 Rockwell Automation 销售顾问合作,以探讨您的软件要求。

联系我们

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation 主页
  2. Chevron LeftChevron Left 产品
  3. Chevron LeftChevron Left 软件
  4. Chevron LeftChevron Left Arena 仿真软件
  5. Chevron LeftChevron Left Arena Simulation Software Case Studies
  6. Chevron LeftChevron Left Improve Personnel Training Procedures