示例:MaxPenNameLength 属性

Private Sub DescribeLineShort() ' Set the description for a pen Trend1.Pens.Item(1).Description = "Temporary" ' Display the line legend on the chart. Trend1.DisplayLineLegend = True ' Show only the first four characters - "Temp" ' Remember - this applies to the whole chart. Trend1.MaxPenNameLength = 4 End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal